Knowledge
Knowledge Center is the best way to find information about MISUMI's technologies and devices.
MISUMI Definition
Camera Appearances

Board Type (B): Module only without any cover, such as Tube, Plastic/ Metal enclosure etc.
Tube Type (T): Camera with a cylinder shape enclosure. Materials may vary.
Forming Type (S): Camera forming by a type of glue or plastic mold enclosure.
Slim Forming Type (Z): Camera forming by a type of glue with specific method.
Plastic Enclosure (N): Camera with a plastic enclosure.
*Appearance can be modified by customer request.

A classification chart of MISUMI camera appearances, showing various types including Board Type (B)、Tube Type (T)、Forming Type (S)、Slim Forming Type (Z)、Plastic Enclosure (N),which can be customized to meet specific requirements.

Camera Orientation Types

Front View: (Bxxxxx) | (Txxxxxx)
Side View: (BLxxxxx) | (TLxxxxx)
Up View: (BxxxxxU) | (TxxxxxU)
Down View: (BxxxxxD) | (TxxxxxD)

 A diagram illustrating various orientation types for MISUMI cameras, including front, side, up, and down views for both board and tube types.

Camera Cable Direction

Front View: Cable Center Out
Side View: Cable Goes Right / Left
Up View: Cable Goes Down
Down View: Cable Goes Up
MISUMI camera module cable direction diagram showing five wiring configurations — center out, up, down, left, and right — with front, side, and product view comparisons for board and tube camera models.

FID Definition
A diagram explaining the focus distance identification (FID) in MISUMI cameras, showing focus ranges and their corresponding values. The FID value indicates the specific focus points and ranges of the camera lens.
Filter Definition

AR: IR PASS (available for B/W camera)
IR: IR cut 645nm (available for color camera)
XR: 850~945nm
YR: 640~940nm,645~850nm cut
       430~600nm & 850~940nm pass
ZR / Z: 800nm [800peak]
ZZR / ZZ: 825~945nm

Camera Parameter Adjustable (UTC Controller)

Camera Parameter Adjustable (UTC Controller)
Model No. UTC-200 Sold Separately
Five Buttons Function

Exposure, White Balance, Day & Night, 
Image Setup, Function Setup, Reset.
(Enter, Up, Down, Left, Right) Toggles.
Camera Parameter Adjustable (5D OSD Key)
Five Buttons Function

Exposure, White Balance, Day & Night, 
Image Setup, Function Setup, Reset. 
(Enter, Up, Down, Left, Right) Toggles.

A comparison of MISUMI's UTC-200 and 5D OSD Key camera controllers, highlighting their five-button interface for adjusting camera parameters such as exposure, white balance, and day/night mode.

Articulation Borescpe

1W series:
Press Controller / One-Way Articulation
2L series:
Lever Controller / Two-Way Articulation
2W series:
Knob Controller / Two-Way Articulation
4W series:
Joystick Controller / Four-Way Articulation

MISUMI articulation borescopes with different controller types: press, joystick, lever, and knob, offering one-way, two-way, and four-way articulations. offering flexible inspection solutions.

Detachable Connector

Detachable Nano Connectors (Customize Option)
Specifically designed to overcome the big size of connector and camera head.
With detachable Nano connectors, a tube can go through the thin cable from halfway.
 Without detachable Nano connectors, camera head cannot go through the tube.

*Each segment can be modified by customer request.

MISUMI's customizable detachable nano connectors allow for a slimmer borescope design, enabling the tube to pass through tight spaces. showcasing the increased flexibility of the nano connector design.

Camera
Depth of Field
The Depth of Field illustrations section visually represents the effects of shallow and deep depth of field, with labels for camera, focus point, background, and focus distance.
Aperture
A diagram comparing the effects of various aperture settings (f-stops) on a photograph, showcasing the relationship between aperture size, depth of field, and exposure.
Binning VGA vs. Crop VGA
Comparison of Crop VGA and Binning VGA image sensors on a MISUMI camera, showing differences in field of view and image quality.
Connectors
MISUMI's diverse connector options, providing solutions for a wide range of electronic devices and applications.
Formula of Image Area and Image Circle (Sensor)
Formula of Image Area and Image Circle (Sensor)

Image Area: 
                    Resolution x Pixl Size = Image Area
                         (H)        x     (H)     = (H)
                         (V)        x     (V)      = (V) 

Image Circle:
√(Image Area)²+(Image Circle)²=  Image Circle Ø
           H                      V                         D

Pixl Size Amount Resolution Sensitivity Power Consumption
Small  More High Low More
Large Less  Low High Less
           
Frame Rate Number Image Speed    
  Small   Bright Slow    
  Large Dark Fast    


A diagram comparing the relationship between pixel size, resolution, sensitivity, and frame rate in an image sensor, as well as the calculation of image area and image circle.
Global vs Rolling Shutter
Global vs Rolling Shutter

Global Shutter
Means that all pixels of the array are exposed simultaneously.
Advantage
• No Distortion of straight lines with fast-moving subjects
• No limit on flash sync speed
Disadvantage
• More noise levels
• Lower frame rates
• Lower dynamic range

Rolling Shutter
Means that adjacent rows of the array are exposed at 
slightly different times as the readout 'waves' sweep through each half of the sensor.
Advantage
• Lower noise levels
• Higher frame rates
• Higher dynamic range
Disadvantage
• Artifacts wit fast-moving subjects
• Limited flash sync speeds

A diagram comparing the advantages and disadvantages of Global Shutter and Rolling Shutter image sensors, highlighting the differences in image quality, distortion, and performance in various conditions.
Hidden Camera with Covers
A diagram illustrating various hidden camera models and their associated components, including different types of screws, buttons, and housings, offered by MISUMI. accessories for discreet surveillance.
Others
UVC Connector & Controller
A diagram showcasing MISUMI's range of UVC connectors and controllers, featuring USB Type A, USB Type C, and USB Type B (OTG) options, along with dimmers and S/F buttons for controlling connected devices.
CVBS Connector & Controller
A diagram illustrating MISUMI's range of CVBS connectors and controllers, including Mini Din, M8, BNC, RCA, Phone Plug, DC, and IRIS types, along with corresponding wiring configurations.
Microphone
A variety of microphone models with different sizes and shapes offered by MISUMI.
Microphone Connectors
A variety of microphone connector models with different lengths and connector types offered by MISUMI.
LED
How to chose?
How do I choose a lens when the camera with lighting?
Camera with LED light source is suggested to use with large aperture F number.
MISUMI APP
MISUMI camera with adjustable parameters via the MISUMI app and AMCAP software.
MISUMI WiFi DVR

WiFi DVR (MP-WF580KP)

All MISUMI UVC Camera are 

Compatible With MP-WF580KP (WiFi DVR)

For example:

Our extremely lightweight 1920 x1080 (1080p)  1/6" CMOS UVC glasses camera 

is compatible with MP-WF580KP (WiFi DVR).

Supports H.264 video format input, loop recording, snapshot functions. 

Supports max memory 128 GB (micro SD).

Users can view live streaming video via a smartphone.

About MP-WF580KP: 

It deliver the best 1080p live streaming performance when using H.264 camera.

MJPEG cameras can only live stream at resolutions of 720p and below. 

MJPEG cameras delivers the best live streaming performance at 640 x 480.

MISUMI's UVC cameras offer seamless integration with the MP-WF580KP WiFi DVR for high-quality live streaming and versatile video recording features.

Android 10 devices do NOT support USB camera connection.
Android 10 devices do NOT support UVC (USB Video Class) devices to be connected in the apps with targetSdkVersion API Level 28 and above.
From November 2019, all app updates on Google Play have been required to target API level 28 or higher.
(source: https://android-developers.googleblog.com/2019/02/expanding-target-api-level-requirements.html) Therefore, for updating the app to Google Play, MISUMI should be API level 28 or higher. Android 10 smartphones CANNOT connect a USB camera like webcams, etc in the app from the Play Store. So far, we haven’t found any official documents form Google OS about these policy changes. We are looking for various ways to solve the issue and will share if there’s any updates.